Posted on July 28, 2004 at 07:30 Hi, Is there any potential risk if i try to write a chunk of data into flash while i am running the code in the flash itself. I am refering to the internal flash of STR71x. It is said that we can write into f...
Posted on July 28, 2004 at 06:50Hi, Is there is recommended RTOS with a small footprint to use with STR71x such that the application code size should be below 64K. Thanx, Anoop