cancel
Showing results for 
Search instead for 
Did you mean: 

In application Flash programming

anoopar
Associate II
Posted on July 28, 2004 at 13:30

In application Flash programming

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
anoopar
Associate II
Posted on July 28, 2004 at 07:30

Hi,

Is there any potential risk if i try to write a chunk of data into flash while i am running the code in the flash itself. I am refering to the internal flash of STR71x.

It is said that we can write into flash as byte or as word, but erasing only as one sector which ll probably be 64K or so and we can write only after erasing. Is there anyway to erase and write into smaller sections in a sector?

Thanks in advance,

Anoop