Posted on May 17, 2011 at 12:51what are the difference between flashloader ver.2.0 and ver.2.1? when using flashloader with different date code of STM32, different flashloader ver.2.0 and ver.2.1 can be seen,
Posted on May 17, 2011 at 12:41This question should be related to IAR EWARM, but I do not know the place of the IAR forum, the question is while enter debugging, the message below shown, or refer to attached file. The C-SPY option ''Run to 'main''' ...
Posted on May 17, 2011 at 12:39 STM32 with 256K flash or above gets hardware SDIO , while 128K or below using SPI to do SD access! major difference between these 2 access? maximum SD capacity access different? possible compatible issue? support futu...
Posted on May 17, 2011 at 12:36STM32F103RBT6 used, out of 5 tries of waking up from stop mode, around 2 times, the program seems continue with a reset state, any idea to check for this problem?