cancel
Showing results for 
Search instead for 
Did you mean: 

only one breakpoint can be set?

hg-chen
Associate II
Posted on August 07, 2008 at 05:49

only one breakpoint can be set?

2 REPLIES 2
hg-chen
Associate II
Posted on May 17, 2011 at 12:41

This question should be related to IAR EWARM,

but I do not know the place of the IAR forum,

the question is while enter debugging,

the message below shown, or refer to attached file.

The C-SPY option ''Run to 'main''' is enabled,but due to a lack of

breakpoints this will require single-stepping ,which may take a long

time.

Do you want to execute anyway,or stop at the first instruction?

only one breakpoint can be set under this condition!

why and how to get it right?

jilisegiar
Associate II
Posted on May 17, 2011 at 12:41

which device are using(STM32, STR9,..)? BTW with the STM32 you can set more than 2 breakpoints.