cancel
Showing results for 
Search instead for 
Did you mean: 

Difference between hardware SDIO and SPI for SD interface?

hg-chen
Associate II
Posted on July 17, 2008 at 19:18

Difference between hardware SDIO and SPI for SD interface?

2 REPLIES 2
hg-chen
Associate II
Posted on May 17, 2011 at 12:39

STM32 with 256K flash or above gets hardware SDIO , while 128K or below

using SPI to do SD access!

major difference between these 2 access?

maximum SD capacity access different?

possible compatible issue?

support future SD card with larger capacity?

16-32micros
Associate III
Posted on May 17, 2011 at 12:39

Hi Kuni,

For SDIO, STM32 High density is fully compatible with SDIO V2.0 and V1.1 and also supports SDHC with larger capacity > 4GBytes and more.

Regards,

STOne-32.