Hello VOANHV, Yes, in fact, the X-NUCLEO-OUT01A2 card is compatible with the NUCLEO-G474RE card, in the same way as it is with the NUCLEO-F401RE or NUCLEO-G431RB cards, because they are in fact Arduino compatible...In addition, for information, the b...
Hello, Effectively, the NUCLEO-WL55JC1 are designed for 865 to 928 MHz frequency bands, and the NUCLEO-WL55JC2 are designed for 433 to 510 MHz frequency bands. The differences between both versions are the external discrete front-end matching between...
Hello,The LC filters in the front end part are used adapt the impedance of the signal coming from the STM32WL transceiver and to ensure that the signal going to the BGS13S4N9 RF Switch is properly filtered. If you bypass the LC filters, and if you co...