Posted on October 22, 2003 at 12:14Hi guys, Have any of you experience with EMC and ST7 microcontrollers? The reason for me asking is that I have several PCBs with ST7 MCUs, which have been mounted close to a 6W 160 MHz radio. The inteference from t...
Posted on September 15, 2003 at 09:20Hi Is it possible to re-program the flash memory of the ST72C334 using the Kanda Keyfob, if the security option has been set to ''No further Read/Write'' in the previous programming? /Ulrich
Posted on June 16, 2003 at 07:40I am using the ST72334 and Metrowerks. Here is the .prm file: /* STACK INITIALIZATION ******************************************************/ STACKTOP 0x01FF /* MEMORY LOCATION SETTING ********************************...
Posted on June 16, 2003 at 05:13Hi I have a problem using the NO_OVERLAP command. I have some local variables which I would like to protect against overwriting. Therefore, I put the #pragma NO_OVERLAP in front of the function as described in the doc...