Hello @johngj
I can't reproduce your error. I'm testing DATALOG2 v2.2.0 with different device_config.json files in the root of the SD card and log never crashed. Can you share the new device_config.json you built up using the Python GUI?
Are you sti...
Hello @johngj
Interrupt lines in FP-SNS-DATALOG2 are working properly. Once a sensor has new data ready, the interrupt pin is toggled. You can see the sensor-related EXTI_IRQHandler invoked during the logging phase only. This is the standard way FP-...
Hello @Batuhan35
Support from BLESensor app depends on the firmware running on the eval boards. Are you sure you've never updated the firmware? Which version of BLESensor app are you using?
There are different examples that can be flashed on both PR...
Hello @JW1
The figure you attached is the Power Spectral Density of the accelerometer data, so it is not true that all figures are in time domain.
HSDPython SDK supports PSD calculation for microphones and accelerometers only.
What are you expecting...