Posted on May 17, 2011 at 10:16I have the same problem. It seems to be caused by a shutdown/turnon sequence between the emulator and software. I usually turn everthing off then back on and then it starts working again.
Posted on May 17, 2011 at 10:16What if any software changes are necessary when changing from a wye connected motor to a delta connected BLDC motor when using the ST72141 processor in sensorless mode?
Posted on July 14, 2006 at 01:56I'm using my own target board with a ST7FMC2R7 processor and a indart incircuit debugger and STVD7 ver 3.0 (based on ST3.1). My serial communication works find, both transmit and receive until I set the CKE bit in MCR...
Posted on April 12, 2006 at 01:09Setting the ST7FMC2R7T6 as PWMCR = 0x00; PADDR = 0x1F; PAOR = 0x0f; PADR = 0x0F; Gives no output on PA0 and PA2 while PA1 and PA3 work The data sheet says these are connected for a TQFP64 device Is this an error ...