cancel
Showing results for 
Search instead for 
Did you mean: 

ST7FMC2R7T6 PA0 and PA2 cannot be configured as PWM or outputs

pjprv1
Associate II
Posted on April 12, 2006 at 01:09

ST7FMC2R7T6 PA0 and PA2 cannot be configured as PWM or outputs

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
pjprv1
Associate II
Posted on April 12, 2006 at 01:09

Setting the ST7FMC2R7T6 as

PWMCR = 0x00;

PADDR = 0x1F;

PAOR = 0x0f;

PADR = 0x0F;

Gives no output on PA0 and PA2 while PA1 and PA3 work

The data sheet says these are connected for a TQFP64 device

Is this an error in the data sheet or just a bad part?