Posted on May 17, 2011 at 11:32The HALT mode has the lowest power consumption mode (typ. 1ua) and it can be exited just by an external reset. Whereas the STOP mode can be exited by one of the 16 external WAKE-UP lines, resuming the code where it was...
Posted on May 17, 2011 at 10:16Hi! I have some questions regarding the ST72141 micro. I am developing a control board for BLDC compressor motor, using this micro and the Kanda kit. My questions are the following: 1) In order to not allow reading the...
Posted on September 25, 2002 at 06:39Hello! You have to be careful; there are some limitations of the ST72F324 device: 1.The Resonator frequency must be 4MHz or higher. At lower frequencies fcpu is not stable. Moreover PLL can be used in the range o...