Posted on May 17, 2011 at 13:06Can I use the I2C Module both as a master and slave at the same time. I need to do this on STM32F101VE. I understand that in I2C slave cannot initiate a data transfer. I have a requirement for bidirectional communicati...
Posted on May 17, 2011 at 13:03Hi, I need to access a 128Mbit SPI Flash interfaced to STM32F101VCT6. What is the address range that I have to use for this device. I have looked up the Memory map for the MCU and it talks about only the ''control and ...
Posted on May 17, 2011 at 12:58I need to connect an external NAND/NOR flash to STM32F101Vx. The option that I am considering is to use is the FSMC interface. In this way this part of the memory will be accesible using the ''uVision'' IDE and related...