User Activity

My current application uses 2 USB ports, both connected to USBPHYC (STM32MP157F). The OTG one is used for programming using CubeProgrammer.My new revision requires 3 USB ports, 2 host and the programming port.According to https://community.st.com/t5/...
I'm having some trouble booting my custom board containing a STM32MP157F. I'm able to program everything using STM32CubeProgrammer, but i'm not able to boot:WARNING: Firmware Image Package header check failed.WARNING: Failed to obtain reference to im...
I'm trying to create a peripheral device that allows one Bluetooth central to connect to it, this part is working. Now I want the device to re-start advertisements when a central has made a connection. The advertisements should be non-connectable one...
I want to readout the STSS22H, without any polling or I2C clock stretching. I want to use the following sequence:Send soft reset commandSend one shot command Release I2C bus for other processes to useWait for the maximum conversion time of the one-sh...
I'm trying to use OOB pairing with the blueNRG1, using the latest DK3.2.1 (stack V2.1c). There is no example available, the security example has all security examples with exception of OOB. I'm trying to use LE legacy mode for now, but LE secure is ...
Kudos from