2022-01-17 5:15 AM
I'm trying to create a peripheral device that allows one Bluetooth central to connect to it, this part is working. Now I want the device to re-start advertisements when a central has made a connection. The advertisements should be non-connectable one's in this case, so I'm not trying to create a device that allows multiple concurrent connections.
I was assuming this would be as simple as just restarting the advertisements with:
ret = aci_gap_set_discoverable(ADV_NONCONN_IND, 160, 160, PUBLIC_ADDR,NO_WHITE_LIST_USE, 0, NULL, 0, NULL, 0, 0); after the connection has been made, so after a call to hci_le_connection_complete_event, but the function returns 0x0C -> BLE_ERROR_COMMAND_DISALLOWED. What am I doing wrong? Why is the command not allowed?
2022-01-27 6:26 AM
Anyone here?
2022-02-04 2:02 AM
Hello,
I don't know if it's possible, but if yes look for aci_gap_init(), with the gap roles
/**
* @anchor gap_roles
* @name GAP Roles
* @{
*/
#define GAP_PERIPHERAL_ROLE (0x01)
#define GAP_BROADCASTER_ROLE (0x02)
#define GAP_CENTRAL_ROLE (0x04)
#define GAP_OBSERVER_ROLE (0x08)