Posted on June 16, 2016 at 15:12Hi Flow and Jerry,I can't yet succesfully send a POST with the httpreq command.I don't understand how you, Flow, used the last \r\n after the json data (do you count or not in the data length for the httpreq?).Actuall...
Posted on June 13, 2016 at 16:20Hi,yes I'll use a external STM32. I was trying the command with a PC utility (Realtherm) because with the external STM32 it didn't work.With your PC utility, the lines you posted are sent all together or separately?If...
Posted on June 10, 2016 at 11:04Hi,This is the command I was sending: at+s.httpreq=192.168.1.174,80,66\rGET / op.php HTTP/1.1\r\nUser-Agent: SPWF01SA1\r\nConnection: close\r\n\r\n\rI was waiting the same response sending the ''at+s.httpget=192.168.1...
Posted on May 30, 2016 at 16:27Hi,I update the module and I'm trying to use the ''httpreq'' command, but without any success.I notice that if I put a comma before the port number (a third one as described in the manual) the module report an ERROR (m...