User Activity

Posted on February 07, 2018 at 13:33 Greetings. I wasted a lot of time trying to figure out what is wrong with I2Ccommunication and thus found this issue. Following code works as it is expected to (it changes corresponding CNFy bits to 0x03 and M...
Posted on October 18, 2017 at 18:06Hello everyone. My current project requires working with NFC and RFID interfaces. I use ST M24SR to interact with NFC-powered smartphones, NXP PN532 to read 13.56 MHz cards and inhouse-designed circuitry for readin...
Posted on October 02, 2017 at 17:36My current project involves some pretty complicated logic, required for firmware update over the air. So I ended up with solution, which contains bootloader and application code, compiled separately. My current mem...
Posted on July 31, 2017 at 18:48Hi, engineers. I am currently working on project, containing SD card. My HW is custom chinese board with STM23f407VET6 mounted and microSD slot connected to SDIO (proper pullup resistors seem to be in place). I made s...
Posted on April 11, 2017 at 18:29I have device model, which consist of stm32f407 discovery board, digital camera and 3.95 inch display with ili9488 controller inside. The display is connected to my stm32 MCU with 8-bit 8080-like bus and accepts RGB5...
Kudos from