Posted on February 05, 2017 at 11:03I am use stm32f429.Me need USB HS connection (speed 480 Mbit/sec) configured as 'Device_Only'.Can I am C for this application?Or me need use external PHY ?OTG not need me.Thank you.
Posted on November 10, 2016 at 15:10Good day! I use microcontroller stm32l476ret. In CubeMX create desired configuration and create project for Keil v.5. The Keil everything compiles without errors. Pour the code into the microcontroller. The mic...
Posted on February 06, 2017 at 06:34I am use stm32f429 really. I am made mistake in the message header. I am can not cerrect it.Me need USB HS connection (speed 480 Mbit/sec) configured as 'Device_Only'.Can I am use internal PHY for this applicatio...
Posted on December 28, 2016 at 12:59Hi!In CubeMX v.4.18.0 this problem present.The OPAMP output pins are configured as GPIO_MODE_ANALOG under HAL_OPAMP_MspInit in stm32l4xx_hal_msp.c while they should be configured as GPIO_MODE_ANALOG_ADC_CONTROL t...
Posted on November 11, 2016 at 09:38Hello, I am not use DMA. I am a little correct file stm32l4xx_hal_adc_ex.c and ADC2 was initialized OK. As I am see any peoples have problem with ADC2 initialization.