Hi @Smalik At my knowledge, there is only one un-direct way to know which wireless stack is embedded.It's by reading the SFSA option byte. This option byte reflects the address in the Flash where the wireless stack has been installed. Wireless stack ...
Dear @GS2 ,At first glance, it sounds like you are trying to run an example on the wrong board.Please, can you clarify where did you find this BLE_HID_Mouse example?Because, on NUCLEO-WB55RG the example is called BLE_HID (without "MOUSE") and the rea...
Hello @onvol2024 ,Let me point to this firmware package which could answer your request:FP-AUD-BVLINKWB1 - STM32Cube function pack for STM32WB MCU featuring full-duplex audio streaming over Bluetooth 5.0 using Opus codec - STMicroelectronicsIn the do...
Many thanks for the feedback.Glad to read that the FUS update went well.Hope it will solve the problem with the P2PServer/Client demo.Best Regards,Alan PorteST MCU Support Team