User Activity

Posted on June 27, 2018 at 21:59Unlike the datasheet for BlueNRG-2 (https://www.st.com/resource/en/datasheet/bluenrg-2.pdf ), the BlueNRG-1 datasheet (https://www.st.com/resource/en/datasheet/bluenrg-1.pdf ) lacks chapter bookmarks. I really miss th...
Posted on June 26, 2018 at 23:21Has anyone else encountered and solved a 'can't halt cpu' issue in IAR EWARM when using the segger j-link to program the BlueNRG-1 part through the 20 pin IDC jtag port on the STEVAL-IDB007V2?  If so could you share t...
Posted on October 27, 2017 at 22:01Is the I-NUCLEO-LRWAN1 extension board plug-in compatible with the STM32F429 Nucleo-144?#lorawan #nucleo-144
Posted on February 07, 2017 at 22:02Is a discovery board available for any of the stm32f417 variants?#stm32f417 #stm32f4-discovery
Posted on January 11, 2017 at 18:02In an IAR/EWARM environment, when I use STM32CubeMX 4.18.0 Project/Generate Code function the program seems to correctly generate its own files but deletes user (that is, my files) from both the EWARM project and f...