HelloIf my understanding is correct, you need to send some additional data link to your IBI.If it is correct, to manage that point you can use the example I3C_Target_InBandInterrupt_IT, which demonstrate the usage of the IBI with additional sent duri...
Hello,Concerning timing calculation for I2C, it is preferable to use STM32CubeMx, as this tool management the timing calculation for all STM32.The calculation of Timing is automatically done through CubeMx, when user select the Input clock frequency ...
hello,Q1:Why is the minimum recommended SDA rise time 350ns? Why do I set 12ns only affect the frequency of 3~5M, which is smaller or higher, why is there no effect?This SDA rise time is the value measure of SDA rise time, between GND to 70%VDD, capa...
Dear,To start better on I3C on H5, prefer modifying only this part of CubeMX at first usage on your side (parameter under yellow highlight):for example, it seems that you modified the default value of SDA rise time, which can be a critical value if n...
Dear,This message is correct in the driver. No issue copy/paste.In fact this message have been added as some "old" I2C slave document shared the address of their device in real 7bits definition. So it will be necessary to shift it to the left to put ...