2017-10-29 9:54 AM
Hello,
in en.stsw-stm8069 firmware for the STM8S001J3 ist not included.
Where can i download it?
Thanks.
2017-10-29 1:58 PM
Hello,
I have checked it and you are right that Standard Peripheral Library for STM8S doesn't include new STM8S001J3 device. It seems that libraries were not updated by us. I am sorry for this inconvenience and thank you for reporting it to us. I will provide this feedback to the team, which is responsible for these libraries.
As a temporary workaround I would recommend you to select the
STM8S003 as used device in Standard Peripheral Library. I used this approach and I didn't have any problems to control ADC, GPIOs, UART and timers ofSTM8S001J3 by fuctions from Standard Peripheral Library
.
Best regards
Szymon
2017-10-31 4:09 PM
Thanks a lot.