2020-09-21 01:19 AM
Hello community,
after unsoldering the solderbridges of the STM8S-Disco-Board, I try to connect the SWIM to a STM8AF Chip. I read in the manueal, that this is not possible (only for STM8S-Family). But after trying it, I could flas Code on the µC and Debug it with the STVD. For example, a counter in my programm ist counting up :-)
But if I want to switch Timer1-Output-Pin from LOW to HIGH, nothing happens.
Is ist possible,, that I can program the µC and it is running without errors, but the mapping of the GPIOs are not correctly done?
Is there a influence of the SWIM-adapter even if I had chosen the STM8AF-Chip in STVD?
Thank you all, Steffen
Solved! Go to Solution.
2020-09-25 12:32 AM
Hello Ozone, hello Community,
I'm sorry, but the problem was on my side:
Our PCB has some defect connections, that was the reason why I could not switch the TIM1 Pin. When I now switch an unconnected pin, I can regulate the output via Software.
So, despite of the hint in the UM 8017 we can use the STM8S-Discoboard SWIM to connect STM8AF µCs
Nevertheless, today I received my ST-LINK-V2 device, so I do not use the discoboard for those purpose anymore.
2020-09-21 04:22 AM
I suppose the firmware of the STM8S SWIM controller on the STM8S-Disco is limited to the S family, most probably because of code/Flash size reasons.
Thus, you are likely running an incorrect configuration.
Perhaps you can "update" the SWIM firmware to that of a STM8AF device.
Had been severeal years since I had been working with STM8s, though.
2020-09-21 07:17 AM
Hi Ozone,
Thank you very much for the quick answer :-)
This is exactly what I'm afraid of. (the incorrect configuration).
Does anyone know, where I can find an "update" from STM8S to STM8AF? On the ST hompage I did not found anything - only updates of the SWIM itself, bur not for different µCs
2020-09-25 12:32 AM
Hello Ozone, hello Community,
I'm sorry, but the problem was on my side:
Our PCB has some defect connections, that was the reason why I could not switch the TIM1 Pin. When I now switch an unconnected pin, I can regulate the output via Software.
So, despite of the hint in the UM 8017 we can use the STM8S-Discoboard SWIM to connect STM8AF µCs
Nevertheless, today I received my ST-LINK-V2 device, so I do not use the discoboard for those purpose anymore.