STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can't connect to STM8L052C6

Hi,I'm attempting to connect to STM8L052C6 with ST-link and receiving an error, "Cannot communicate with the device !"I've read every forum post on google related to the issue and tried just about everything to connect.Finally I found in the manual f...

0693W000005AX9pQAG.png 0693W000005AX9zQAG.png
CDarw.1 by Associate II
  • 2017 Views
  • 7 replies
  • 0 kudos

cosmic compiler error?

hiComsic STM8 compiler suite version: 4.4.12.I am using this compiler version together with ST's STVD.In the sample code attached, with line 13 conditional define set to 0, the compiler yields compilation error (my intended implementation), and the a...

Keeloq firmware

In DT0094, KeeLoq RX application over S2-LP, the following is mentioned:KeeLoq firmware example for RX node available on request through local marketing / sales representative.Has anybody got a copy of this?

VTrea.1 by Associate
  • 643 Views
  • 0 replies
  • 0 kudos

STM8S003F3 - flash endurance and lab classes

Hello,The STM8S003F3 is a Value Line device with quite small number of write/erase cycles. The data sheet says:Program memory: 8 Kbyte Flash memory; data retention 20 years at 55 °C after 100 cycles---My wife is going to use very cheap W1209 thermost...

About STM8S Flash block write

The chip I use is STM8S003F3. When using Flash block erase, it is executed in RAM. If the offset of the Flash address is used with a 32-bit variable, the execution will cause an error. Can this 8-bit microcontroller use 32-bit addressing in RAM?

LXiao.11 by Associate
  • 615 Views
  • 0 replies
  • 0 kudos