2024-11-26 11:25 AM
This started last week and is making it take 30-60 seconds to load and save my workspace. Also, the top menu bar containing the items for File, Edit, View, Debug, Project ... is missing! I can do Alt+F and Alt+P but I'd like it restored.
Right clicking a toolbar shows an endless list of choices. Sure enough if I open the workspace .WED file which is 700k it contains all these entries:
[WorkState_v1_2.DockState]
Bars=1192
.....
And 1192 childbar entries! If I delete this file after closing the workspace, these all return when I load and save again. Something is corrupted and I can't find anything in my files or registry to fix either issue. The other 3 workspace files appear to be fine.
This is making it hard to continue my work. I've already switched to the STM8 from NXP S08 and I do not want to switch again because of the quality of the tools.
Solved! Go to Solution.
2024-12-02 9:30 PM
Deleting the WDB and WED files that have the same name as the workspace restored the file menu and restored the loading and saving speed. I was forced to keep looking for a solution to this because it was taking 60 seconds to start debugging and over 90 to stop debugging. I don't know what made this occur but one thing I had enabled was large toolbar icons before I noticed the file menu missing. Unchecking large icons did not restore it.
2024-12-02 9:30 PM
Deleting the WDB and WED files that have the same name as the workspace restored the file menu and restored the loading and saving speed. I was forced to keep looking for a solution to this because it was taking 60 seconds to start debugging and over 90 to stop debugging. I don't know what made this occur but one thing I had enabled was large toolbar icons before I noticed the file menu missing. Unchecking large icons did not restore it.