2024-03-23 10:27 AM
I have a very simple main using UART1 and already my application is 7kB! The web implies that this is because I am getting a lot of UART1 and CLK code built and linked in that I am never using. One suggestion is to split the UART1 and CLK files into individual "one file per method" codebases, build a library, and then when my application links it will pull in only those methods that I am actually using.
However I cannot see how to configure a project to build a library instead of an image. Could someone point me an example of how to do this please?
2024-03-23 11:49 AM
I think you are using COSMIC compiler. COSMIC linker can remove unused code even without a library and without split the code into individual files "one file per method". Read COSMIC manual.
Use +split compiler option to create a separate sub-section per function. To create a library use clib utility.
How do you know your application uses 7KB of FLASH?
2024-03-24 4:58 AM
Thanks for the COSMIC tip - I will go and look.
The 7KB value came from the size of the resulting `s19` file. For comparison, having not yet checked out your suggestions but having `#defined` out UART functions that I am not using, the `s19` file is now 2.4kB.
Am I misunderstanding how the size of these `s19 files relates to the about of flash used for store the program on the stm8s? I'm new to these processors.
Thanks.
2024-03-24 5:14 AM
Another newbie question. I have enabled `+simple` at compile time but the linker requires me to also enable `-k` against a segment. I was hoping to find a compile time macro that would allow this but didn't find one so in the context of the STVD IDE, how do I do this?
Thanks.
2024-03-24 12:14 PM
s19 file is not a binary file. s19 file size if more than twice the code size.
You can see code size in map file.
2024-03-24 12:16 PM
I don't know '+simple' compiler option. Maybe you want '+mods0' compiler option.
2024-03-25 4:10 AM
Bother - I meant `+split`.
2024-03-31 5:56 AM
What I did with this was...
- Added `+split` to the compiler options
- Added `-k` to the linker segment options for the `.const` segment.
This seem to have done the trick as the mapfile now contains likes like this:
_UART1_ClearFlag ******** *** removed from Debug\stm8s_uart1.o ***