STM8S003F3 reset pin - output frequency
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-02-26 10:24 PM
Posted on February 27, 2015 at 07:24
1. I have made a circuit using STM8S003F3.
I don't understand somehow when I probe reset pin of MCU, it is giving 12Khz freq output.
Thus I am unable to program/debug the MCU.
2. I have removed everything else from board. Just +5V supply & MCU.
MCU supply is decoupled by 0.1u & 1u caps.
Vcap pins is decoupled by 1uF cap.
Reset pin is decoupled by 0.1uF cap.
That's it . Nothing else on circuit.
3. I have probed VCC pin of MCU, I get clean +5V across it.
Probing Vcap pin gives +2V clean.
I have also removed 0.1u cap from reset pin & then checked the bare pin but same result.
Edit: I have also changed 2 MCU but same results
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0