2015-02-23 9:27 AM
I'm running
ST library IEC60335 STM8AS v1.1.0 in a STM8S105C6.RAM March X periodic test is failing, I think there is an error in the library.Class B RAM (fromCLASS_B_START=0x10 to CLASS_B_END=0x7F) is checked from TIM4 interrupt by ''ClassBTestStatus STL_TranspMarchX(void)'' function.
Firstly it copies 6 bytes from Class B RAM to RunTimeRamBuf[RT_RAM_BUF_SIZE] @ ''RUN_TIME_RAM_CHCK''. Section RUN_TIME_RAM_CHCK is placed at 0x00-0x0F.
This is the loop that copies 6 bytes from Class B RAM to RunTimeRamBuf:
/* ------------------ Regular memory Self-check ----------------------- */
/*---------------------------- STEP 1 --------------------------------- */
/* Save the content of the 6 bytes to be tested and start MarchC-
Write background with addresses increasing */
p_StartRamBlock
=
p_RunTimeRamChk;
p_EndRamBlock=
p_RunTimeRamChk
+
RT_RAM_BLOCKSIZE;
i=
1u
;
do
{
RunTimeRamBuf[i
++
]
=
*
p_RunTimeRamChk;
*
p_RunTimeRamChk
++
=
BCKGRND;
}
while
(p_RunTimeRamChk
<
p_EndRamBlock);
p_StartRamBlock and p_EndRamBlock are local variables placed at virtual registers (0x80…).
p_RunTimeRamChk is a global variable placed at Class B RAM, my linker places it @0x10. This variable is used in the above loop that copies Class B RAM and then writes BCKGRND (=0) in it, so the loop is writing to the variable that controls the loop. Result: it starts copying 6 bytes from 0x10 to 0x01 and writing 0 from 0x10 to 0x15, but when the loop writes 0 in 0x10 it is writing 0 in p_RunTimeRamChk. The loop copies more than 6 bytes and RAM is corrupted.
Is there an error in this library certified by VDE????
Regards
2015-02-24 8:57 AM
p_RunTimeRamChk & its inversion should be placed OUTSIDE the ''CLASS_B'' sections precisely because of the problem you're seeing.
jdf2015-02-26 12:56 AM
OK John, but this variable is placed inside class B RAM in the ST library. Maybe it must be there because it is mandatory. I use a local variable that holds its value while RAM is being tested.
I think there are more errors, the loop writes outside class B RAM, so RAM is again corrupted, etc.I hope it is my mistake, or I can't believe this library is VDE certified.Best regards2015-02-26 8:46 AM
Here is a snippet from stm8s_stl_classB_var.h where p_RunTimeRamChk and its inversion are definitely declared in section .RUN_TIME_BUF.. I'm quite confidant in the library itself (I have one project certified under UL60730 using it & another in progress) however the demo projects as provided by ST seem to leave out some important stuff. For example the Cosmic demo projects stm8_903.stp and stm8s_105.stp do not declare the RUN_TIME_BUF section. Not to mention changing the linker files around which I've always found a particular challenge. I use Cosmic for stm8 & st7 development so cannot offer opinions on others. (well I could and often do, but they'd be of no value).
If you continue to have difficulty send a copy of your project file(*.stp) and any changes you've made to stl_classB_var.h & I'd be happy to take a look. Have fun jdf /** ****************************************************************************** * @file stm8s_stl_classB_var.h * @brief This file contains definition all class B variables * @author STMicroelectronics - MCD Application Team * @version V1.1.0 * @date MAY-2012 ****************************************************************************** * @copyright * * <h2><center>© COPYRIGHT 2012 STMicroelectronics</center></h2> * * Licensed under MCD-ST Liberty SW License Agreement V2, (the ''License''); * You may not use this file except in compliance with the License. * You may obtain a copy of the License at: * * http://www.st.com/software_license_agreement_liberty_v2 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an ''AS IS'' BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ /* Define to prevent recursive inclusion -------------------------------------*/ #ifndef __STL_CLASS_B_VAR_H #define __STL_CLASS_B_VAR_H #include ''stm8s_stl_param.h'' /* This avoids having mutiply defined global variables */ #ifdef ALLOC_GLOBALS #define EXTERN #else #define EXTERN extern #endif /* Includes ------------------------------------------------------------------*/ /* Exported types ------------------------------------------------------------*/ /* Exported constants --------------------------------------------------------*/ /* Exported macro ------------------------------------------------------------*/ /* Exported functions ------------------------------------------------------- */ /* Global variables --------------------------------------------------------- */ /* Temporary RAM buffer used during transparent run-time tests */ /* WARNING: Real reserved RAM location from 0x.... to 0x.... */ /* ==============================================================================*/ /* MISRA violation of rule 8.5 - Class B variables are defined at one place only defined just at begin of stm8l_stl_startup.c file, all other files include this header as a common reference */ #ifdef _IAR_ #pragma diag_suppress=Pm123 #endif /* _IAR_ */ #ifdef _COSMIC_ #pragma section @near [RUN_TIME_BUF] /* Buffer to store original RAM content during run-time tests */ EXTERN @near u8 RunTimeRamBuf[RT_RAM_BUF_SIZE]; /* RAM pointer for run-time tests */ EXTERN @near u8 *p_RunTimeRamChk; EXTERN @near u8 *p_RunTimeRamChkInv; #ifdef STL_VERBOSE EXTERN @near u16 FreqDifDisplay; // Not really a Class B variable, but useful for debugging #endif /* STL_VERBOSE */ #pragma section @near [CLASS_B] EXTERN NEAR u16 MarchOverlayGap; /* gap in memory due to March test overlay */2015-02-26 9:23 AM
Thank you John
Variables are defined for 3 compilers and they are placed in different sections, the Cosmic definition seems good, but take a look at the IAR definition:#ifdef
_IAR_
EXTERN__near
u8 RunTimeRamBuf[RT_RAM_BUF_SIZE] @
''RUN_TIME_RAM_CHCK''
;
/* RAM pointer for run-time tests */
EXTERN__near
u8
*
p_RunTimeRamChkB @
''CLASS_B_RAM''
;
EXTERN__near
u8
*
p_RunTimeRamChkInv @
''CLASS_B_RAM_REV''
;
#ifdef
STL_VERBOSE
EXTERN__near
u16 FreqDifDisplay;
/* Not reallya Class B variable, but useful for debugging */
#endif
/* STL_VERBOSE */
EXTERN NEAR u16 MarchOverlayGap @''CLASS_B_RAM''
;
/* gap in memory due to March test overlay */
EXTERN__near
u16 CtrlFlowCnt @
''CLASS_B_RAM''
;
/* program flow execution at start */
EXTERN__near
u16 ISRCtrlFlowCnt @
''CLASS_B_RAM''
;
/* program flow execution in interrupt */
EXTERN__near
u16 LSI_HSIStartUpFreqkHz @
''CLASS_B_RAM''
;
/* First measure LSI over HSI stored */
EXTERN__near
u16 LSI_HSEStartUpFreqkHz @
''CLASS_B_RAM''
;
/* First measure LSI over HSE stored */
EXTERN__near
u16 LSI_StartUpPeriod @
''CLASS_B_RAM''
;
/* Initial measure of LSI - reference for run-time checks */
EXTERN__near
u16 TickCounter @
''CLASS_B_RAM''
;
/* Sofware time base used in main program (SysTick ISR) */
EXTERN__near
volatile
u8 TimeBaseFlag @
''CLASS_B_RAM''
;
/* Indicates to the main routine a 100ms tick */
EXTERN__near
u16 LastCtrlFlowCnt @
''CLASS_B_RAM''
;
/* Control flow counter from one main loop to the other */
EXTERN__near
const
u8
*
p_RunCrc16Chk @
''CLASS_B_RAM''
;
/* Pointer to FLASH for crc16 run-time tests */
EXTERN__near
u16 CurrentCrc16 @
''CLASS_B_RAM''
;
/* Current FLASH 16-bit Crc */
EXTERN__near
u16 CurrentDesc @
''CLASS_B_RAM''
;
/* Current Descriptor Address */
EXTERN__near
u16 CRCBlockIndex @
''CLASS_B_RAM''
;
/* Counter needed for partial CRC test */
EXTERN NEAR u16 MarchOverlayGap_ @''CLASS_B_RAM''
;
/* gap in memory due to March test overlay */
EXTERN__near
volatile
u8 StackOverFlowPtrn[
4
] @
''STACK_BOTTOM''
;
/* Magic pattern for Stack overflow in this array */
EXTERN NEAR u16 MarchOverlayGapInv @''CLASS_B_RAM_REV''
;
EXTERN__near
u16 CtrlFlowCntInv @
''CLASS_B_RAM_REV''
;
EXTERN__near
u16 ISRCtrlFlowCntInv @
''CLASS_B_RAM_REV''
;
EXTERN__near
u8 LSI_HSIStartUpFreqkHzInv @
''CLASS_B_RAM_REV''
;
EXTERN__near
u8 LSI_HSEStartUpFreqkHzInv @
''CLASS_B_RAM_REV''
;
EXTERN__near
u16 LSI_StartUpPeriodInv @
''CLASS_B_RAM_REV''
;
EXTERN__near
u16 TickCounterInv @
''CLASS_B_RAM_REV''
;
EXTERN__near
volatile
u8 TimeBaseFlagInv @
''CLASS_B_RAM_REV''
;
EXTERN__near
u16 LastCtrlFlowCntInv @
''CLASS_B_RAM_REV''
;
EXTERN__near
const
u8
*
p_RunCrc16ChkInv @
''CLASS_B_RAM_REV''
;
EXTERN__near
u16 CurrentCrc16Inv @
''CLASS_B_RAM_REV''
;
EXTERN__near
u16 CurrentDescInv @
''CLASS_B_RAM_REV''
;
EXTERN__near
u16 CRCBlockIndexInv @
''CLASS_B_RAM_REV''
;
EXTERN NEAR u16 MarchOverlayGapInv_ @''CLASS_B_RAM_REV''
;
#endif
/* _IAR_ */
I think
p_RunTimeRamChkB
placement is wrong for IAR compiler.
Should I use Cosmic compiler?Best regards2015-02-27 9:28 AM
Hi
When I read your post my initial reaction was to recommend you use the compiler you're most familiar with. But after looking at the IAR parts more closely I'm not sure. If you're looking for certification under UL they won't blindly accept the VDE certificate so you could fix the IAR stuff though I'm not sure where I'd start as I've only used IAR with the Samsung Sam8. I'm using Rev1.0.3 which was current when I started & going through UL had to test everything anyway so the lack of VDE wasn't an issue. I did try to compile the demo projects for Rev1.1.0. Only the 103 & 207_208 would build. The 105 & 903 errored out at link time because segment RUN_TIME_BUF isn't defined. Easily fixable though. This is typical of my experience with ST provided code. Not well documented & tested and best avoided if you can. STVD though is my favorite IDE. Of course I only use it for compiling & debugging but rarely use foul language while doing so. I'm really sorry I couldn't give you some definitive answer. Use Cosmic if you can, the 16k free version is good. jdf2015-02-27 11:48 AM