2024-04-10 3:33 AM
I am using the STM8S bootloader via a USB/FTDI. I can use Wireshark/USBpcap and catch the exchanges and I have a somewhat happy "export packets, parse with Python" method of looking at the exchange.
But has anyone already written a proper Wireshark dissector for this?
2024-04-10 5:11 AM
It seems, STM8 has no DFU bootloader. So I understand you that you have a serial to USB converter in between STM8 and PC and you want to spy on the USB side? Why dont you spy on the serial lines? Did you have a look at STM8 Flash loader demonstrator (UM0462,AN2606 and AN3155))? Protocoll seem similar to STM32 serial bootloader. Maybe stm32flash can be modified? What are you trying to achieve anyways?
2024-04-10 5:20 AM - edited 2024-04-10 5:30 AM
I have already implemented the bootloader for an stm8s but the uploading a new app failed. By catching the exchange between the flasher and bootloader using Wireshark/USBpcap, exporting the frames and then writing a quick-n-dirty python script I was able to see that it is the "write" operation failing.
Of course I could capture the data by getting more hardware and monitoring the serial lines instead of the USB traffic, and then writing a custom capture tool and dissector but it I'm going to go to that trouble I figured why not just use existing tools and write a Wireshark dissector directly since Wireshark/USBpcap can already monitor the flows for me.
But of course if someone else has already written the Wireshark dissector, I would not need to even write a Wireshark dissector :-).