cancel
Showing results for 
Search instead for 
Did you mean: 

mqtt resources

francescatodiego
Associate II

Posted on June 12, 2015 at 16:38

If someone is interested in developing devices that use protocol MQTT leave some information about what I have  done (... not my code ....my boss fire me)

 

In attachment the protocol specifications (I am sorry I forget where I download the document)

Here http://www.hivemq.com/downloads/

 

The mqtt broker for windows or linux (I work with windows version) very simpe start... ''run.bat''

Well documented conf directory contain all config parametersall well explained in site doc

The broker open the standard ports 1883 or 8000 for websockets

With wireshark you can monitor the traffic and save lot of time for debug

My wireshark version 1.12.5 support mqtt dissector and all message are full decoded

 

Form here: http://ftp.acc.umu.se/mirror/eclipse.org/paho/1.0/

I have downloaded org.eclipse.phao.mqtt.utility.1.0.1.jar

Small mqtt client used for subcribe topic and checking mi device mqtt publishing

 

#mqtt-protocol

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
qwer.asdf
Senior
Posted on June 12, 2015 at 16:54

Thank you for sharing your knowledge.

> ... not my code ....my boss fire me

Fortunately, there is open source code available, like

https://github.com/AvengerGear/chibios-stm32f407-discovery-mqtt

project.
francescatodiego
Associate II

Posted on June 12, 2015 at 19:09

Oh yes another source

http://git.eclipse.org/c/paho/org.eclipse.paho.mqtt.embedded-c.git/

(but not for ST)

But the code is not mine, I am paid to write it, and it does not seem correct to publish it.

I wanted to give the ''public information'' to faciltiare who will develop  applications with MQTT.

I do not know if the code ready to use can be used in commercial products that do not include the release of the code.