2019-09-25 1:41 PM
Hi,
For me to set the SWIM pin to (Input Float NO), I need to set all ports attached to pin 1, as follows:
* NAME |DDR |CR1 |CR2 |ODR | Operation |FUNC
* PA.0 - 0 - 0 - 0 - 0 - Input Float NI - SWIM
* PA.2 - 0 - 0 - 0 - 0 - Input Float NI - SWIM
* PC.6 - 0 - 0 - 0 - 0 - Input Float NI - SWIM
Or I can just set one of the ports attached to pin 1, any of them, like:
* NAME |DDR |CR1 |CR2 |ODR | Operation |FUNC
* PA.0 - 0 - 0 - 0 - 0 - Input Float NI - SWIM
What is the way to configure a pin of this microcontroller? Do I have to configure only one PIN port or do I have to configure all PIN ports?