cancel
Showing results for 
Search instead for 
Did you mean: 

STM8L-Discovery Debugging

stm8
Associate II
Posted on January 21, 2011 at 08:27

Hello,

I use the ST Visual Develop IDE together with the Cosmic Compiler and the STM8L-Discovery.

Everything seems to work fine, besides the debug function.

When I try to start debugging I get the following error message:

''Connection error (usb://usb): swim error [30200]: st-link connection error''

I found discussions of Linux users about this topic, but I use Windows...

Any idea how I get this to work?

Thanks in advance.
10 REPLIES 10
filip
Associate
Posted on January 03, 2012 at 21:46

Hi, after playing with the toolset dll, i've found out the following:  first i took a copy of the stvp folder. installed 4.3 and replaces all stlinkusbdriver.dll (v4.2.2.0) with the old version (v4.0.1.2). Stangly the new V4.2.2.0 is only 64Kb while the old one is 380Kb in size. So it is possible that some other conflics arrive with this change...