Skip to main content
Rokyy
Associate
July 12, 2019
Solved

stm8af5288 nrst pin 1K resistance?

  • July 12, 2019
  • 1 reply
  • 1357 views

Will the external 1k resistor of the nrst pin have an effect?

    This topic has been closed for replies.
    Best answer by Sisto Zànier

    In the worst case, the internal pull-up resistor may have a minimum value of about 30K , so when you generate a Reset, the effective voltage level of NRST input, will be (VCC/31K)*1K = 0,106V

    This value is much lower than the maximum level of 0.8V, required to reset the STM8Lxx.

    Therefore all voltages below this value will generate a microcontroller reset.

    Instead, I don't know how your MCU reset is generated, but if you really want to insert a 1K resistor in series at the NRST input, it would be better if it was placed before the 100nF by-pass capacity.

    In this way you would also have a certain filter effect.

    1 reply

    Sisto Zànier
    Senior
    July 16, 2019

    In the worst case, the internal pull-up resistor may have a minimum value of about 30K , so when you generate a Reset, the effective voltage level of NRST input, will be (VCC/31K)*1K = 0,106V

    This value is much lower than the maximum level of 0.8V, required to reset the STM8Lxx.

    Therefore all voltages below this value will generate a microcontroller reset.

    Instead, I don't know how your MCU reset is generated, but if you really want to insert a 1K resistor in series at the NRST input, it would be better if it was placed before the 100nF by-pass capacity.

    In this way you would also have a certain filter effect.