2024-01-18 2:07 AM - edited 2024-01-31 2:18 AM
Hello everyone, i've an issue using STM8L with an SPBTLE-RF bluetooth module.
It seems that the module stop to transmits data to the master after few time of utilization or during an intensive use.
I verified that when the module stop to transmits data, the INTERRUPT_HANDLER function which call the HCI_Isr function doesn't work.
The code of the INTERRUPT_HANDLER function:
INTERRUPT_HANDLER(EXTI3_IRQHandler, 11)
{
// Call to manage the packet received from the BlueNRG
HCI_Isr();
}
Anyone know why this happen and how can i fix it?