2013-09-06 03:39 AM
I am trying to load program using STVD (ST-Link/V2) but getting the error ''can't communicate with the device''.
I am only applying Vcc and Gnd to controller + 4 wires of SWIM cable. What should I do? Do I need to use external Pull up resistor on reset pin? #st-link/v2-programming-issue2013-12-17 10:09 PM
Hi, I too had same problem but a simple logic , use 1microF capacitor betweeb 7and 8 pins (Vss and Vcap) . Then try to program . it will definateley work check for loose connections also.
2013-12-19 11:03 PM
Yes.... that was the problem..
Thanks..!!!!!!