STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L low power run mode

Posted on December 04, 2013 at 08:49Hello. We are developing a low power product that uses STM8L151 MCU. The product is in low power run mode when on idle stage and program is executed from RAM. I was wondering that how reliable is this functionalit...

taneli by Associate
  • 723 Views
  • 1 replies
  • 0 kudos

STLux 385 ?

Posted on April 16, 2012 at 15:14Has anybody information about the STLux 385 ? This is assumed to be a STM8 based controller, especially targeted to lighting applications. Even ST as producer seems to obliviate any knowledge ... #ride #digital-po...

New Release Raisonance C Compiler for STM8

Posted on December 03, 2013 at 14:36For Raisonance STM8 compiler, RLink and EvoPrimer users... New release of Raisonance software tool set for STM8 available supporting new STM8AL ultra-low-power series for automotive applications including: . STM8...

Good bye, STM-8?

Posted on April 27, 2013 at 08:19Just received a letter from Raisonance(aka KEOLAB). They changed their license policy. Their 32kb-limited compiler isn't free anymore. It costs (TADAAAM!!) 700 euro per computer. The only alternative is cosmic compil...

elijah by Associate III
  • 1080 Views
  • 2 replies
  • 0 kudos

Why IAR can't add source file of StdPeriph_Drive

Posted on November 26, 2013 at 15:43I have uncommend all the Periph_Drive, but the compiler still do not compile their source file. Why there are some source file are gray? I want to use TIM1, but the compiler keeps tell me the function inside it ha...

0690X00000603OPQAY.jpg

STM8L152C6T6 - Temperature sensor pin

Posted on November 25, 2013 at 14:58Hello everyone, I can't find the relative pin to the internal temperature sensor. Does anyone know which pin is it? Or should i only configure the TSON bit in the ADC_TRIGR1 register to wake up the temperature sen...

gibba by Associate II
  • 779 Views
  • 2 replies
  • 0 kudos

stand alone SWIM programmer/sample code?

Posted on November 17, 2013 at 22:48I suddenly find that we need a couple of stand alone programmers for our STM8L052 board. By ''stand alone'' I mean the application code will have to be loaded into the programmer and it will flash the production u...

tim by Associate
  • 646 Views
  • 1 replies
  • 0 kudos

STM8S103K3 Drop in replacement for STM8S003K3?

Posted on November 21, 2013 at 20:05I plan to use the STM8S003K3 in my product.  However the flash has a life of only 100 cycles.This makes it impractical to use during development.  The STM8S103K3 looks like an exact substitute - is it?Is there any...

How to achieve real low power?

Posted on November 18, 2013 at 14:47I'm looking to build a small application which wakes up the uC each 500ms to handle some software loops, and then go back in active halt mode with RTC (alarm and wake up function enabled) and LCD running with LSE....

STVD hangs on build

Posted on November 19, 2013 at 18:21I have encountered an issue with STVD which is persistent also in the latest version (4.3.4). The issue seems to be pre-compilation (my guess would be generation of the project.lkf file), but I'll get to it in a m...

shabbyx by Associate II
  • 690 Views
  • 0 replies
  • 0 kudos