RTC clock not starting consistenly
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-08 9:28 AM
Hi everyone, I'm using the STM8L152R8 Nucleo board and trying to get the RTC running on the LSE clock. It works but only inconsistenly, about 2/3 runs error out in the RTC_EnterInitMode function of the SPL the below line. RTC_EnterInitMode is called from RTC_Init which I call in my setup.
if ((RTC->ISR1 & RTC_ISR1_INITF) == RESET)
{
status = ERROR;
}
My setup is
while (CLK_GetFlagStatus(CLK_FLAG_LSERDY) == RESET);
/* wait for 1 second for the LSE Stabilisation */
/* Select LSE as RTC clock source */
CLK_RTCClockConfig(CLK_RTCCLKSource_LSE, CLK_RTCCLKDiv_1);
CLK_PeripheralClockConfig(CLK_Peripheral_RTC, ENABLE);
RTC_InitTypeDef RTC_InitStr;
RTC_InitStr.RTC_HourFormat = RTC_HourFormat_24;
RTC_InitStr.RTC_AsynchPrediv = 0x7F;
RTC_InitStr.RTC_SynchPrediv = 0x00FF;
RTC_Init(&RTC_InitStr);
//setup calender
I can see from the registers that the LSE is setup correctly however the RTC is not setup at all.
Can anyone suggest what is happening here?
Thanks!
- Labels:
-
RTC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-09 1:36 AM
I removed the timeout which has solved the issue though I'm not certain why.
From the manauls init steps :
' Poll INITF bit of in the RTC_ISR register. The initialization phase mode is entered when INITF is set to 1. It takes around 2 RTCCLK clock cycles for synchronization purposes.'
The timeout was '0xFFFF' which should be more than enough time for 2 RTC clock cycles with LSE at 32.768 kHz and HSI at 16 MHz.
If anyone can shed some light on this it would be appreciated. Thanks