2021-04-07 2:54 AM
Hi,
while the software are working, suddenly it will become stop, and reset pin is permanently forced low, it freaks me out!! Someone will help me, thank you so mutch
2021-04-07 3:26 AM
what do you mean with permanently?
2021-04-07 4:44 AM
Thank you Javier
reset pin goes to 0 Volt and doesn't work until the power is off. It seems to be frozen.
this appens especially when we are getting strong electric interference
2021-04-07 4:46 AM
Thank you Javier
reset pin goes to 0 Volt and doesn't work until the power is off. It seems to be frozen.
this appens especially when we are getting strong electric interference
2021-04-07 5:21 AM
@fcasa.16 maybe show us some pictures/schematics or explain a little bit more your issue.
2021-04-07 12:46 PM
And the GPIO next to the RESET pin?
Also, what chip do you use? On some you can change the RESET pin into PA1.
2021-04-07 11:05 PM
MCU: STM8L151C8T6 , below section of schematic, RESET, after power on, change in PA1 Output OD and SWIM change in PA0. I'm at my wits end
2021-04-07 11:11 PM
Is it possible to NOT re-use RESET and SWIM? Because my guess is that your problem has something to do with that. I never use those pins for anything else than programming and debugging. If I need more pins than available I upgrade to a bigger microcontroller.
So (if possible) see if the problem still happens when you don't do anything with PA0 and PA1.
2021-04-08 1:09 AM
Unfortunately, problem still happen even if I not reuse reset and swim.
2021-04-08 2:32 AM
Without having the pcb and code here it is hard to guess. It can be all sorts of things, floating GPIO doing strange things, a short between another pin and the RESET line, an error in the code causing the RESET to be pulled low...
Single stepping through the code isn't possible I think, because you said the microcontroller will work for a while, you might be single stepping for ages. Maybe logging things, for example by sending data out via a uart and recording it with Notepad++ will give you some clues.