2021-05-27 2:04 AM
I tried this code on STM8S001J3 with 8 pins:
/* MAIN.C file
*
* Copyright (c) 2002-2005 STMicroelectronics
*/
//#include “stm8s.h�?
/*main()
{
while (1);
}
*/
#include "STM8S.h"
void clock_setup(void);
void GPIO_setup(void);
void TIM1_setup(void);
void delaySomeTime(void);
void main(void)
{
//signed int i = 0;
clock_setup();
GPIO_setup();
//TIM1_setup();
while(TRUE)
{
GPIO_WriteReverse(GPIOB,GPIO_PIN_4);
GPIO_WriteLow(GPIOB,GPIO_PIN_5);
GPIO_WriteLow(GPIOC,GPIO_PIN_5);
GPIO_WriteLow(GPIOD,GPIO_PIN_6);
delaySomeTime();
GPIO_WriteReverse(GPIOB,GPIO_PIN_4);
GPIO_WriteHigh(GPIOB,GPIO_PIN_5);
GPIO_WriteHigh(GPIOC,GPIO_PIN_5);
GPIO_WriteHigh(GPIOD,GPIO_PIN_6);
delaySomeTime();
}
}
void delaySomeTime(void){
int i = 0;
int j = 0;
for(i = 0; i < 100; i++){
for(j = 0; j < 100; j++){
//;
_asm("nop"); //Perform no operation //assembly code
}
}
}
void GPIO_setup(void)
{
GPIO_DeInit(GPIOB);
GPIO_Init(GPIOB, GPIO_PIN_4, GPIO_MODE_OUT_PP_HIGH_FAST);
GPIO_Init(GPIOB, GPIO_PIN_5, GPIO_MODE_OUT_PP_HIGH_FAST);
GPIO_DeInit(GPIOC);
GPIO_Init(GPIOC, GPIO_PIN_5, GPIO_MODE_OUT_PP_HIGH_FAST);
GPIO_DeInit(GPIOD);
GPIO_Init(GPIOD, GPIO_PIN_6, GPIO_MODE_OUT_PP_HIGH_FAST);
}
void clock_setup(void)
{
CLK_DeInit();
CLK_HSECmd(DISABLE);
CLK_LSICmd(DISABLE);
CLK_HSICmd(ENABLE);
while(CLK_GetFlagStatus(CLK_FLAG_HSIRDY) == FALSE);
CLK_ClockSwitchCmd(ENABLE);
CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);
CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);
CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSI, DISABLE, CLK_CURRENTCLOCKSTATE_ENABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_I2C, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_SPI, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_ADC, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_AWU, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_UART1, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER1, ENABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER2, DISABLE);
CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER4, DISABLE);
}
/*void TIM1_setup(void)
{
TIM1_DeInit();
TIM1_TimeBaseInit(16, TIM1_COUNTERMODE_UP, 1000, 1);
TIM1_OC1Init(TIM1_OCMODE_PWM1,
TIM1_OUTPUTSTATE_ENABLE,
TIM1_OUTPUTNSTATE_ENABLE,
1000,
TIM1_OCPOLARITY_LOW,
TIM1_OCNPOLARITY_LOW,
TIM1_OCIDLESTATE_RESET,
TIM1_OCNIDLESTATE_RESET);
TIM1_CtrlPWMOutputs(ENABLE);
TIM1_Cmd(ENABLE);
}*/while, the LEDs didn't blink as it were expected, why? (I used SPL in STVD and programmed in STVP by ST-Link V2.)
2021-05-27 2:05 AM
I used SPL in STVD and programmed in STVP by ST-Link V2.
2021-05-27 10:28 AM
I don't comment on your code, but how do you expect the LEDs to blink? How do you test if it works?
Do you expect to see a blinking with the eye?
Your delaySomeTime() function would take around 2,5 ms - you cannot see this with the bare eye.
2021-05-27 3:19 PM
I set "i < 1000" and "j < 1000" before, it was the same.