cancel
Showing results for 
Search instead for 
Did you mean: 

Option Byte Programming - Critical

Dileep P D
Associate II

Hi,

I am trying to program the option byte in STM8S003 controller. I am able to do the same using STVP tool. It is not a practical method on production, so want to add the option byte config in the source code. for that I added the below code snippet. But it is not happening properly. Please help me to fix this issue, correct me if I am doing wrong.

#define AFR_OPTION_BYTE_ADDR 0x4803

#define AFR0_ENABLE 0x01

void set_afr0_option_bit(void)

{

uint16_t option_status;

uint8_t option_byte=0;

option_status=FLASH_ReadOptionByte(AFR_OPTION_BYTE_ADDR);

printf("\n\rOption Byte Status = %04x ",option_status);

if(!(option_status & 0x0100))

{

//option_status |= 0x0100;

option_byte = (uint8_t) AFR0_ENABLE;

FLASH_ProgramOptionByte(AFR_OPTION_BYTE_ADDR, (uint8_t)AFR0_ENABLE);

printf("\n\rOption Byte updated successfully = %02x ",AFR0_ENABLE);

}

option_status=0;

option_status=FLASH_ReadOptionByte(AFR_OPTION_BYTE_ADDR);

printf("\n\rOption byte status %04x ",option_status);

}

The debug output is

------------------------------------

Option Byte Status = 00ff

Option Byte updated successfully = 01

Option byte status 00ff

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0