2009-01-28 1:30 AM
max input frequency
2011-05-17 6:02 AM
Hi I.Yeganeh,
I have tried this example using Internal Clock source HSI (16Mhz), and it works correctly, I suggest you to change the input value of frequency and Try the example, this the only way to understand why it has been 50Mhz Best Regards Bassinux2011-05-17 6:02 AM
Hi
maximom clock input frequency parameter for stm8s micro is 24 MHZ (datasheet) but I2C_EEPROMReadWrite example in the stm8sfwlib filder input clock frequency set to 50MHZ. why is this?2011-05-17 6:02 AM
Hello l.yeganeh,
The maximum frequency available for the I2C peripheral on STM8S is 24MHz. It can not be more as it is the maximum input frequency of the MCU. Best regards, Seb