cancel
Showing results for 
Search instead for 
Did you mean: 

Marking STM8L151F3U6TR

Zalila_2021
Associate

Hi, I have bought the parts STM8L151F3U6TR. The marking indicated in datasheet is L526. However, marking on component is L536. Anyone can confirm this marking of L536 is correct? 

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @Zalila_2021, to the community!

As can be seen in the data sheet, fig 53, L526 is only a marking example and stands for the STM8L151F2U6.

The STM8L151F3U6TR is in fact marked with L536.

Please remember: the 10-year product longevity of the STM8 is running, but they have been on NRND since the beginning of 2022 and should be replaced urgently for longer running projects.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Zalila_2021, to the community!

As can be seen in the data sheet, fig 53, L526 is only a marking example and stands for the STM8L151F2U6.

The STM8L151F3U6TR is in fact marked with L536.

Please remember: the 10-year product longevity of the STM8 is running, but they have been on NRND since the beginning of 2022 and should be replaced urgently for longer running projects.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.