cancel
Showing results for 
Search instead for 
Did you mean: 

Identify this component - LIS344ALH?

Matt_UK
Associate

Hi,

 

Are you able to identify the below products from their product markings?  I believe they should both be the LIS344ALH but one of them is behaving strangely. The 34AH marked product is reading 1g (2.332V) in the z axis when placed flat on a desk. The ones with markings 34AL are reading 0.7g (2.117V) when in the same position. I have switched the ICs around to rule out a PCB fault, but the difference always follows the IC, suggesting there is a difference between the AL and AH marking. I can't find any details on the datasheet outlining product markings to understand the codes printed on top of the IC.

 

 A057 - 20250203_115100.bmpA055 - 20250203_111204.bmp

 

Thanks

 

Matt

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @Matt_UK, to the community!

I am extremely sorry to have to inform you that the LIS344xx accelerometers have long been discontinued and that STMicroelectronics no longer has any information about them. As sensor markings are/were also still internal information, you will probably not find any information in the vastness of the otherwise never-forgetting internet.

I am very sorry not to be able to give you more pleasant information.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @Matt_UK, to the community!

I am extremely sorry to have to inform you that the LIS344xx accelerometers have long been discontinued and that STMicroelectronics no longer has any information about them. As sensor markings are/were also still internal information, you will probably not find any information in the vastness of the otherwise never-forgetting internet.

I am very sorry not to be able to give you more pleasant information.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AScha.3
Super User

The chips from rs also have  AH marking:

AScha3_0-1738591630317.png

So just replace the chips with wrong marking.

If you feel a post has answered your question, please click "Accept as Solution".