2010-01-15 10:09 AM
Linker errors while compiling any of sample project in STVD
2011-05-17 6:06 AM
Hello,
I am looking for some help with the following issue: Running Linker clnk -l''C:\Program Files\COSMIC\CXSTM8_16K\Lib'' -o Debug\discover.sm8 -mDebug\discover.map Debug\discover.lkf #error clnk Debug\discover.lkf:27 can't open file crtsi0.sm8 #error clnk Debug\discover.lkf:47 can't open file libis0.sm8 #error clnk Debug\discover.lkf:48 can't open file libm0.sm8 The command: ''clnk -l''C:\Program Files\COSMIC\CXSTM8_16K\Lib'' -o Debug\discover.sm8 -mDebug\discover.map Debug\discover.lkf '' has failed, the returned value is: 1 exit code=1. discover.elf - 5 error(s), 0 warning(s) Same thing while trying to build ADC sample. Help much appreciated. Thank you!2011-05-17 6:06 AM
Thank you mozra,
It appears that for some reason all of my tool paths contained a series of non alfanumeric characters at the end. I was able to copy the setting from my colleague. Many thanks! Kamil2011-05-17 6:06 AM
Well, whenever something says that it ''can't open'' a file, you have to ask yourself why - don't you?
Have you checked that these files exist on your PC? If they do exist, have you checked that the tools are correctly configured to find them?2011-05-17 6:06 AM
Hi,
you can update your cosmic path(Tools>Options>Toolset>Root path) as following C:\Program Files\COSMIC\CXSTM8_16K (remove Lib directory from the path) Regards mozra2011-05-17 6:06 AM
Hi mozra27,
it seems this is a bug of latest STVD version: STVD MainFrame Version 3.6.4.2 - Build Dec 17 2009 stvabbld.dll, Version: 1.3.3.0 stv7abbld.dll, Version: 1.4.3.0 STVD_TxtEditor.dll, Version: 1.0.2.5 addonide.ini, Version: Rel 4.0, Date: 19 February 2008 ProgrammerAddOn.dll, Version: 1.3.0.1 st7expor.dll, Version: 3.3.4.0 when migrating on this new version I had the same problem: I had to specify manually root path for Cosmic, and it was not the case before. brazov2