2019-09-25 6:21 AM
In a project I'm working on, I am using the internal EEPROM of the STM8L151.
I do not initialize the variables (of course), but the compiler automatically set them all to 0. This is a bit of a problem because my code looks for 0xFF to see whether or not the variables have been previously written. And with 0 being a valid value for most of them, this distinction cannot be made.
Now, I realise that in production this is no big deal, because I can simply just not program the EEPROM, but in debugging it is a right royal pain in the neck.
I have gone through the Cosmic documentation, but couldn't find anything.
So, does anyone have a solution?
Best regards,
Rob
2019-09-25 7:12 AM
I don't know Cosmic compiler specific, but according to the C standards, a value of 0 is assumed if you do not initialize global/static variables.
That means, outside of function scope,
int myVariable;
is equivalent to
int myVariable = 0;