cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a STM8 model that has a parallel external RAM interface?

Vyacheslav Azarov
Associate III
Posted on September 11, 2017 at 09:15

Hello. Answer please. Is there a STM8 model that has a parallel external RAM interface? Thank you in advance.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Philipp Krause
Senior III
Posted on October 23, 2017 at 14:13

Well, I guess, everyone looks at the question, doesn't know about any STM8 with parallel RAM interface (I definitely don't know about any), but are not sure that none exists, so no one answers?

Philipp

Posted on October 23, 2017 at 16:24

I was hoping to get a specific answer from the developers.

Pavel A.
Super User
Posted on October 28, 2017 at 01:06

Do you mean, external memory bus like in 8051? Nope :( They do not have enough pins.

-- pa

Posted on October 28, 2017 at 06:34

Yes. The 8-bit micro-controllers Atmel and Microchip is supported external memory interface. However, I could not find such an opportunity for STM8, even for high-density devices