2018-07-16 12:32 AM
ST has recently introduced 8-pin STM8 devices, while previously the lowest pin count available was 20.
I would like to see more STM8 devices with relatively low pin count, e.g. 12 or 14 pins. Since I intend to replace an Elan Microelectronics EM78P153A �C by an STM8, a compatible pinout would be great, but any 12- or 14-pin device would be good.
Are there any plans to introduce further STM8 devices with less than 20 pins?
Philipp
#stm8s001 #em78p153a #low-pin-count #new-device2018-08-08 06:52 AM
Bumping to remove from the home page (No Answer Posts)
ST has sale staff/organization that can provide customers with forward looking and roadmap information. Call the local office, or your distributor