2020-09-23 6:55 AM
2020-09-24 10:45 AM
Right, " Some info might help".
2020-09-24 11:22 AM
Here it is in stm8_it.c
INTERRUPT_HANDLER(EXTI_PORTB_IRQHandler, 4)
{
/* In order to detect unexpected events during development,
it is recommended to set a breakpoint on the following instruction.
*/
if((GPIOD->IDR & GPIO_PIN_3)!=0){
state = TRUE;
} else
{
state = FALSE;
}
}
This is how it's setup now for Pin 3 of PortD for interrupt. I want to add another interrupt to the same Port D at Pin 4.
I did a bitwise OR for these two pins if((GPIOD->IDR & GPIO_PIN_3) !=0 || (GPIOD->IDR & GPIO_PIN_4) !=0) ) but there's no result.