cancel
Showing results for 
Search instead for 
Did you mean: 

How to initialise the RTC on STM8L151K4T6

JEdmu.1
Associate

Hi All,

This is my first MCU project attempt and figured I would build a 7-segment clock. I have managed to write a little bit of code to configure the GPIOs in the way that I want them as well as the system clock, but I cannot for the life of me figure out how to get the RTC up and running (after reading the notes in the source file). I seem to have slammed into a wall at the RTC_Init stage.

My current system clock setup is this:

void clk_setup (void){

//Disable the CLK, ready for setup

CLK_DeInit;

//Set Hi-Speed Internal to On

CLK_HSICmd(ENABLE);

//Set Hi-Speed External to off

CLK_HSEConfig(CLK_HSE_OFF);

//Set Lo-Speed Internal to on

CLK_LSICmd(ENABLE);

//Wait for Busy flag to go low

while(CLK_GetFlagStatus(CLK_FLAG_LSIRDY) == FALSE);

//Set Lo-Speed External to ON 32,768Khz

CLK_LSEConfig(CLK_LSE_ON);

//Wait for Lo-speed external busy flag to go low

while(CLK_GetFlagStatus(CLK_FLAG_LSERDY) == FALSE);

//Set System Clock to Hi-Speed-internal

CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_HSI);

//Set System clock Divider to 8

CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_8);

//Set RTC Clock to Lo-speed-external. 

//Set RTC Clock divider to 1

CLK_RTCClockConfig(CLK_RTCCLKSource_LSE, CLK_RTCCLKDiv_1);

//Set RTC Clock Peripheral to Enable

CLK_PeripheralClockConfig(CLK_Peripheral_RTC, ENABLE);

//Set LSE CSS to on

CLK_LSEClockSecuritySystemEnable;

//Set RTC Failure mode to on

CLK_RTCCLKSwitchOnLSEFailureEnable;

//Set configurable clock output to off

CLK_CCOConfig(CLK_CCOSource_Off, CLK_CCODiv_1);

//Turn on UART clock

CLK_PeripheralClockConfig(CLK_Peripheral_USART1, ENABLE);

//Turn on ADC clock

CLK_PeripheralClockConfig(CLK_Peripheral_ADC1, ENABLE);

}

Any help with the getting the RTC up and running is appreciated, though bare in mind, I am completely new to this programming lark :beaming_face_with_smiling_eyes: , My last clock was all 4000 series logic :face_with_tears_of_joy:

Cheers

John

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0