2022-03-20 01:37 AM
As the result, the right side has very short run (it reaches 1023 in one sixth of travel). The same for Y axis, the same with another joystick. Both joysticks work properly with arduino - middle 520 (or so). Is there any (obvious) reason; how can I remedy this?
Thanks!
SOLVED:
I connected +5V pin of the joystick to +3.3V pin of the MCU - works properly now!