cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, Where to get the Source Code of the EVAL Board STEVAL-ILD004V2 with STM8S103F2 Controller? Can anybody help me? Best Regards, Walter

WMaca
Associate II
 
2 REPLIES 2
AvaTar
Lead

The link to the firmware provided seems to be a "short circuit": https://www.st.com/content/st_com/en/products/embedded-software/evaluation-tool-software/stsw-ild004fw.html

Perhaps approach ST directly (FAE or via distributor).

I tried to load the demo firmware from ST using ST visual programmer but I got the error below.

Error : Cannot communicate with the device !

Check the SWIM cable connection and check all the needed pin connections on the SWIM connector.

If the application code uses Swim Disable and Reset pin as Output or has disabled SWIM Clock Divider:

Try Now to SWITCH OFF and ON the application Power Supply while NRST Reset pin is forced low.

Regards,

Walter Macamos